DOCA0258EN-00

Firmware Upgrade Page Body

To update the firmware of the LTMT main unit, LTMTCT/LTMTCTV sensor module, and LTMT expansion modules, proceed as follows.

  1. On the Firmware Upgrade section, click Browse to choose the firmware package file from your PC.

    NOTE: The standard web server supports only files with .sedp extension.
  2. Click Upgrade to start the firmware upgrade.

    Result: An Uploading message appears.

  3. Click OK.

    Result: A Package verification in progress message appears.

  4. Click OK.

    Result: An update successful message appears.

    NOTE: If no new firmware is available, No Firmware to Update message appears.
  5. If the update is successful, Firmware Update Failed message appears. Repeat the procedure to update the firmware.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?