DOCA0258EN-00

Overview

The Maintenance page provides an option to upgrade the firmware of LTMT main unit, LTMTCT/LTMTCTV sensor module, and LTMT expansion modules, ensuring they operate with the latest features, improvements, and security updates.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?