Block Output
The table lists the block output for the Modbus TCP/IP and EtherNet/IP communication.
|
Modbus TCP/IP Address (Register) |
EtherNet/IP Address |
RW |
X |
Unit |
Type |
Range |
Default value |
Svd |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x0ED6 (3799) |
83 : 03 : 31 |
RW |
1 |
– |
UINT16 |
|
0 |
Y |
Function setting |
|
0x0ED7 (3800) |
83 : 03 : 32 |
RW |
0.01 |
s |
UINT16 |
0–60000 |
0 |
Y |
Contactor or Breaker open time |
|
0x0ED8 (3801) |
83 : 03 : 33 |
– |
– |
– |
– |
– |
– |
– |
Reserved |