250929_LSS100100/LSS100200_SW_03.0

User Management

The USER MANAGEMENT tab displays a list of the users created in the controller's user interface (Configurator > User access > Add new user).

NOTE: You cannot add users in the USER MANAGEMENT tab. You can only manage their access to the Management plugin functions. If you want to add new users, you must do so within the Configurator plugin.

Steps to manage user access:

  1. Navigate to the USER MANAGEMENT tab in the Management plugin.

  2. Select the user whose access rights you want to configure.

  3. Click the pencil icon at the end of the user's row.

  4. In the Editing user dialog box, enable or disable access to the following functionalities:

    • Controller Sharing

    • Device API

    • Remote Configuration

    • Cloud Access

    • Modbus Profiles

  5. Click Save to apply the changes.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?