250929_LSS100100/LSS100200_SW_03.0

API Description

The Swagger API description is available without enabling the API itself. It can be found at https://<IP>/api/management/v1/swagger.json.

As the API features may vary with different versions, the attached Swagger YAML file in this document may not precisely match what is available on your device.

IMPORTANT: Always update the application for the latest features and security fixes.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?