250929_LSS100100/LSS100200_SW_03.0

Management Plugin

This section introduces and provides a user guide for the Management plugin (controller application).

The Management plugin integrates key functionalities for experienced controller application users. It supports both independent operation and guidance from a system integrator. Users can modify settings within individual tabs, providing enhanced flexibility.

The Management plugin includes the following tabs:

USER MANAGEMENT

This tab allows registered controller users to manage access to individual functionalities within the Management plugin.

CONTROLLER SHARING

This tab enables the cloud/mobile app account holder to manage access for other accounts (similar to the Home Management functionality available in the mobile application).

DEVICE API

This tab allows you to enable the REST API, which provides access to the controller's low-level administrative functions and settings. Do not confuse with the KNX IoT 3rd Party API Local or Cloud.

REMOTE CONFIGURATION

This tab will only be enabled when your controller has been assigned a SpaceLogic KNX Remote service subscription. Available through eConfigure/ETS, this feature allows the system integrator to securely access your controller remotely and configure your KNX project or controller.

CLOUD ACCESS

Create or log in to a cloud account here.

MODBUS PROFILES

This tab allows you to manage Modbus profiles in the controller, including downloading from the cloud and updating or removing profiles.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.