250929_LSS100100/LSS100200_SW_03.0

Installation

You can install the Management plugin directly from the Marketplace or via a binary file with a signature for controllers outside the public network.

Install from Marketplace

  1. Access your controller’s landing page at https://<IP>/ and click in the upper right corner of the screen to enter the Marketplace.

  2. In the list of available applications, find the one called Management and click to install the plugin.

NOTE: It is recommended that you enable the automatic updates feature to ensure that you always have the latest version installed.

Install via Binary File and Signature

If you have obtained the necessary files (with .ipk and .sig extensions) from a trusted source, follow these steps:

  1. Access the Marketplace from your controller’s landing page (https://<IP>/).

  2. Click in the upper left corner and select Install from file.

  3. In the pop-up menu, select the Package file (.ipk) and Signature file (.sig) and click OK to install.

NOTE: Never install the plugin without the signature file to avoid serious security risks.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?