250929_LSS100100/LSS100200_SW_03.0

Device API

The Management plugin allows you to enable an internal REST API that provides access to the controller's low-level admin functions and settings.

This API provides a subset of the functionalities available in the Configurator, including backing up and restoring projects, retrieving logs, viewing CPU loads, and more.


IMPORTANT: For security reasons, ensure you set a strong password for the controller. Enabling the REST API opens access to low-level admin functions and settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?