250929_LSS100100/LSS100200_SW_03.0

Cloud Access

This tab allows users to create their own cloud account or log in to the existing cloud account linked to their controller. A cloud account is required for specific functions, such as access to the Wiser KNX app, voice control, SpaceLogic KNX Remote.

Create an Account/Login to the Cloud

  1. Click the Management plugin icon on your controller's landing page (https://<IP>/app) to open it.

  2. Navigate to the CLOUD ACCESS tab and click the Login to cloud button.

  3. Follow the form for registration or login provided by the remote service.

    NOTE: You cannot be logged into two accounts simultaneously on two computers.

  4. Once logged in or registered, you will be redirected back to the Management plugin. Three cloud action buttons will replace the Login to cloud button once your controller is authenticated:

    • Unpair controller

    • Log out

    • Delete account

Log Out and Delete the Account

If your controller is authenticated, you can log out or delete your account.

NOTE: You will need your cloud account password to delete the account. Deleting the account is irreversible.
  1. Navigate to the CLOUD ACCESS tab.

  2. Click the Log Out or Delete account button as needed.

Pair/Unpair Controller

If your controller is authenticated, you can also pair or unpair the current controller. Pairing the controller is possible only within 5 minutes after a controller reboot. To pair the controller, reboot the device.

Once paired, you can unpair it by clicking the Unpair controller button.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.