250929_LSS100100/LSS100200_SW_03.0

Example of API Call

Here is an example of an API call to retrieve the system hostname:

curl --location 'https://<IP>/api/management/v1/flashsys/system/hostname' \
--header 'Accept: application/json' \
--header 'Authorization: Basic <BASIC_TOKEN_ADMIN>'

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.