250929_LSS100100/LSS100200_SW_03.0

Modbus Profiles

In this tab, you can manage Modbus profiles on the controller. You cannot add profiles by uploading a file. They can only be added from the cloud.

The MODBUS PROFILES tab has the following sections:

  1. Available profiles: This section displays available for download from the cloud. You can add a profile to the controller by clicking on the right side of the profile row.

  2. Updatable profiles: This section shows profiles that have updates available.

    • Download the profile to your local storage.

    • Update the profile.

    • Delete the profile.

  3. Up to date on controller: This section lists all updated profiles on the controller.

    • Download the profile to your local storage.

    • Delete the profile.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?