System Requirements
To ensure optimal performance and compatibility with IFTTT, please make sure you meet the following system requirements:
Hardware |
Wiser for KNX or spaceLYnk controller |
Ensure you have a hardware version greater than 2. |
Firmware |
Latest firmware |
Make sure you have the latest firmware installed. The latest firmware is available for download at se.com. |
Software |
Plugins |
Ensure the Cloud Connector and KNX IoT 3rd Party API plugins are installed and enabled (enabled for Cloud). Enabling automatic updates is recommended to ensure you always have the latest version of these plugins installed. |