MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Activating Extended Settings for Dimming

To activate the extended settings for dimming, you must enable them here.

Master/Ext. 1/2 Output 1 – 2: Dimming

Express settings for dimming

 
 

Extended settings for dimming

No

Yes

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?