MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Staircase Lighting Time Function (Staircase Timer)

This function is used to switch on a consumer, for example, the light in a staircase, via a bus telegram (dimming up) and automatically switch it off again after a set duration (dimming down). Therefore, no manually or automatically generated bus telegram is required for switching off. The actuator carries out the switching off operation independently and under time control.

Two types of staircase lighting time function are available:

Master/Ext. 1/2 Output 1 – 2: Dimming

Staircase lighting time

Time settings

Staircase lighting time

Disabled

Fix

Variable

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?