MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Scenes

If you want to change multiple room functions simultaneously at the press of a button or with a command, you can do so using the scene function.

You can use a scene, for example, to switch on the room lighting, set the heating control to daytime operation and control the blinds.

Without the scene function, you would have to send a separate telegram to each actuator to get the same setting, since these functions can not only have different telegram formats, but also the telegram values have different meanings (e.g. value "0" for lighting OFF and for OPEN blind).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?