MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Incandescent Lamps

The following dimming curve is stored for incandescent lamps:


Dimming curve: Incandescent lamps

You will find the parametrized dimming range on the Y-axis.

The minimum brightness (Minimum Brightness) and maximum brightness (Maximum Brightness) can be limited.

The KNX value range (0-100%) is located on the X-axis.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?