MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Automatic Calibration

Each time the drive moves to the defined end position due to a positioning command, the calibrating function is performed. This means that a running time allowance of 5% of the total running time is added to the calculated travel time required by the drive to ensure that the drive reliably reaches the desired end position. Once the end position has been reached, the movement counter is also reset.

Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

-Blind/roller shutter

Calibration

-Automatic, Locking & Calibration settings

Automatic calibration

Upper

Lower

Upper and lower

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?