Drive Behavior after End of Weather Alarm
Once the sensor values of the weather sensors have returned to the normal measuring range, the weather alarms are deactivated again. You can define a reaction to be performed by the drive as soon as there is no longer any weather alarm active:
The drive then performs the following functions:
-
No reaction: the drive remains in its current position. The alarm function is terminated.
-
Up: the drive moves to the upper end position. The alarm function is terminated.
-
Down: the drive moves to the lower end position. The alarm function is terminated.
-
Move to position prior weather alarm: the drive returns to the position it had before the weather alarm. The alarm function is terminated.
-
Accept current automatic position: this setting is only useful if the automatic function is active. The drive moves to the last automatic position requested. The alarm function is terminated.