MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Priority

The safety function is a 1-bit group object with the highest priority. This means that this object takes precedence over the following group objects:

Alarm object / Lock object / Priority object Priority of Functions for Switching

Logical input object

Scene object

Central switch object

Staircase fix / Staircase variable object

Switch object

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?