Defining Channel Functions
Each dimming output can be can be defined as the channel function Enabled or Disabled.
With an MTN6805-0008, SpaceLogic KNX Switch/Blind Extension, each output can be operated in the function Disabled or Switch or Blind or Roller shutter. In blind and roller shutter operation, two outputs are grouped together to form a single channel. The output contacts of the relays are then electronically interlocked. This means that you cannot switch on both contacts of a motor channel simultaneously. This applies to control via bus telegrams and to manual operation on the device.
|
General settings |
Channel function for Master | ||
|
Dimming Output 1 |
Disabled Enabled |
||
|
Dimming Output 2 |
Disabled Enabled |
||
After activation of Extension 1
MTN6810-0102 Universal Dimming
|
General settings |
Channel function for Extension 1 | ||
|
Dimming Output 1 |
Disabled Enabled |
||
|
Dimming Output 2 |
Disabled Enabled |
||
MTN6805-0008 Switch/Blind
After activation of Extension 2
MTN6810-0102 Universal Dimming
|
General settings |
Channel function for Extension 2 | ||
|
Dimming Output 1 |
Disabled Enabled |
||
|
Dimming Output 2 |
Disabled Enabled |
||
MTN6805-0008 Switch/Blind