MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Status Response for Brightness Value

Master/Ext. 1/2 Output 1-2: Dimming

Express settings for dimming

 

Status response for value

Disabled

Enabled

The value of the signal object of a channel always corresponds to the current output value. The object value is sent in the following cases:

  • A dimming process is terminated.

  • The minimum or maximum dimming value has been reached.

  • A dimming process was stopped by manual operation.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?