MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Lock of Automatic Mode

If operation with equal priorities for manual operation and automatic mode is not always suitable for your application, you can disable and re-enable automatic mode using an additional object as required:

Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

-Roller shutter

Automatic, Locking & Calibration settings

-Automatic, Locking & Calibration settings

Automatic mode

   

Lock of automatic mode

Disabled

Enabled

   

Automatic locking

At object value "1"

At object value "0"

   

Status of automatic locking

Disabled

Enabled

   

Behavior on deactivating automatic locking via object

No reaction

Accept current automatic position

Once the function “Lock of automatic mode” and “Status of automatic locking” has been enabled, new group objects are available for the channel.

  • The feedback object sends a “1” if automatic locking is active.

  • The feedback object sends a “0” if automatic locking is inactive.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?