MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Priority

Relay states caused by higher-priority functions take precedence over behavior after ETS download.


Example:
OR logic operation with parameterized value of the logic object after bus voltage recovery = 1, prevails and switches the output.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?