MTN6710-0102S / MTN6810-0102 / MTN6805-0008

For Your Safety

DANGER
Risk of fatal injury from electric shock, explosion or arc.
Safe electrical installation must be carried out by qualified professionals.
Qualified professionals must demonstrate an in-depth knowledge of:
  • Connecting to installation networks
  • Connecting multiple electrical appliances
  • Installation of electric cables
  • Connection and setup of KNX networks
  • Commissioning KNX installations
  • Safety standards, local connection rules and regulations
Failure to follow these instructions will result in death or serious injury.

The devices and the associated ETS application must not be used to control safety-related applications.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?