Group Objects for Operating Hours Counter
|
No. |
Name |
Object function |
Length |
Behavior |
Data Type |
|---|---|---|---|---|---|
|
31 |
Master/Extension 1/2 Output 1/2 |
Operating hours |
4 bytes |
Sending |
13.100 time lag (s) |
|
32 |
Master/Extension 1/2 Output 1/2 |
Lifetime exceeded |
1 bit |
Sending |
1.005 alarm |
|
33 |
Master/Extension 1/2 Output 1/2 |
Reset operating hours |
1 bit |
Receiving |
1.015 reset |
The Lifetime exceeded object: If the number of operating hours exceeds the value set in the Operating hours limit parameter, the output sends value 1. The output has value 1 until you reset the operating hours with the Reset operating hours object.
If the Reset operating hours object receives value 1, the operating hours for the load are reset,
and the object Lifetime exceeded is set to
value 0.