MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Drive Behavior after the End of Movement Restriction

If the limitation of the movement range is determined by object values and a new object value cancels an active limitation, then you can operate the drive normally again. If the drive is to perform an automatic action in this case, you can define it with the following parameter:

Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

-Blind/roller shutter

Movement range limits

-Automatic, Locking & Calibration settings

Behavior at the end of movement restriction

No reaction

Up

Down

Move to position prior to movement restriction

Accept current automatic position

Values to be set:

  • No reaction: the drive remains in its current position.

  • Up: the drive moves to the upper end position.

  • Down: the drive moves to the lower end position.

  • Move to position prior to movement restriction: the drive returns to the position it had before the movement restriction.

  • Accept current automatic position: this setting is only useful if the automatic function is active. The drive moves to the last automatic position requested.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?