MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Enabling a Central Function for Each Output

Master/Ext. 1/2 Output 1 – 2: Dimming

Express settings for dimming

 
 

Central function

Enabled

Disabled

The global settings and explanations of the central function can be found in the chapter Enabling Central Functions.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?