MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Same Dimming Time at Central Function and Scenes

The function Same dimming time causes a dimming process with several dimming channels to start simultaneously and to end at the same time. You can use this function for scenes and central functions.

Extended settings

Global settings for dimming

Same dimming time for central function and scenes

No

Yes

Same dimming time for central function and scenes(6s - 59.999 min)

6 s

   

Control same dimming time via bus

No

Yes

The group object appears after the enabling Control same dimming time via bus.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?