MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Behavior after Download

After the ETS download, the output can adopt a parametrized state.

If an internal defect or a faulty download results in a state in which the application is not operational, the device will not react.

If you wish to activate the behavior after ETS download for an output channel, you must set the parameter Output at end of download.


Possible settings:

  • No reaction
    The output channel remains at its current brightness value.

  • Switch Off
    The output channel is switched off.

  • Switch on at selectable brightness
    The initial brightness is determined by another parameter. The selectable brightness can be set between 1% and 100%.

  • As before download
    The output executes the behavior set before the download. Any subsequent manual switching is overwritten. If a higher-level function (priority or lock) is active, the behavior you defined for these functions will be executed.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?