MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Contact Mode Normally Opened

The settings for Output 1 are described below, but apply equally to all outputs.

Ext. 1/2 Output 1-8 -Switch: Switching

Express settings for switching

 
 

Contact mode

Normally opened

Normally closed

If the switch object receives a telegram with the value “0”, the contact is opened. If a telegram value of “1” is received, the contact is closed.

The settings “Pressed” and “Released” are used for the different switching states of the output contacts.

In relay mode “Normally opened”:

  • Pressed = contact closed

  • Released = contact opened


Switching (Normally opened mode)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?