MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Reaction on Receipt of Manual Object Value

Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

-Roller shutter

Automatic, Locking & Calibration settings

-Automatic, Locking & Calibration settings

Automatic mode

   

Reaction in automatic mode on receipt of a manual object value

Automatic mode remains enabled

Automatic mode disabled

Automatic mode temporarily disabled

   

Deactivation time for automatic mode

1 min (1 min - 24 h)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?