MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Movement Range Limits

Movement Range Limits

Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

-Blind/roller shutter

Movement range limits

-Automatic, Locking & Calibration settings

Movement range limits

Disabled

Enabled

   

Limit movement range

Immediately after bus voltage recovery

At object value "1"

At object value "0"

   

Feedback for range limitation

Disabled

Enabled

Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

-Blind/roller shutter

Movement range limits

-Automatic, Locking & Calibration settings

Limit movement position

Limit range at lower position

 

   

Upper limit value in % (fix)

0

   

Lower limit value in %

100 (0-100)

   

Limit movement position

Limit range at upper position

   

 
   

Upper limit value in %

100 (0-100)

   

Lower limit in % (fix)

0

   

Behavior at the end of movement restriction

No reaction

Up

Down

Move to position prior to movement restriction

Accept current automatic position

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?