MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Relay Behavior after Bus Voltage Failure

If the bus voltage falls below 18 V, the drive can be switched to a parameterized state. The drive can either be defined as stopped (Stop) or remain in the state it had before the failure (No reaction). At the same time, the current position of the relay is saved in the device.


Possible settings:

  • No reaction: the drive remains in its current state, i.e. it remains stationary or it continues to execute a current movement until the running times have elapsed.

  • Stop: the drive stops immediately.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?