Behavior after Download
After the ETS download, the relay can adopt a parameterized state.
If an internal defect or a faulty download results in a state in which the application is not operational, the device will not react. The output relays remain in their last position.
If you wish to activate the behavior after ETS download for an output channel, you must select a “relay state at end of download” for each channel.
Possible settings:
As before download:
The
relays execute the behavior set before the download. Any subsequent
manual switching is overwritten. If a higher-level function (logic
operation, priority control or lock) is active, the behavior you defined
for these functions will be executed.
Pressed:
In the case of
a normally opened contact, the relay is closed; in the case of a normally
closed contact, the relay is opened.
Released:
In the case of
a normally opened contact, the relay is opened; in the case of a normally
closed contact, the relay is closed.