MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Behavior After Bus Voltage Recovery

Using the parameter Behavior after bus voltage recovery, you can define the reaction of the channel to bus voltage recovery and the output state:


Disabled
Priority remains deactivated. The switching state of the channel results from the other higher-level functions or from the set switching behavior after bus voltage recovery.


Enabled, Off
The priority is automatically activated on bus voltage recovery and the output is switched to "Off".


Enabled, On
Priority is automatically activated on bus voltage recovery and the output is switched to "On".


As before bus voltage failure
The priority is brought to the state it had before the bus voltage failure. If the priority was previously active, the output is switched to the state it had previously.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?