MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Central Function Roller Shutter

Central Function for Blind

The global settings and explanations of the central function can be found in the chapter Enabling Central Functions.

Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

-Roller shutter

Express settings for roller shutter

 

Central function

Enabled

Disabled

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?