MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Weather Alarm Function

The weather alarm function can be activated for all roller shutter/blind channels in the ETS.

There are now 5 different weather alarms available, together with their group objects.

The monitoring of the signals of the activated weather sensors can be carried out cyclically. The device then expects a telegram from the relevant sensor within the cycle time set. If such a telegram is not received within the monitoring time, the associated weather alarm is nevertheless triggered for safety reasons (if, for example, the sensor or the cable connection between sensor and blind channel is defective and no message would be sent in the event of a genuine alarm).

Extended settings

Global settings for roller shutter and blind

 

Weather alarm function

Disabled

 

Enabled

Monitoring time for wind alarm 1

Disabled

   

1 s ... 12 h

 

Monitoring time for wind alarm 2

Disabled

     

1 s ... 12 h

   

Monitoring time for wind alarm 3

Disabled

     

1 s ... 12 h

   

Monitoring time for rain alarm

Disabled

     

1 s ... 12 h

   

Monitoring time for frost alarm

Disabled

     

1 s ... 12 h

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?