MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Switching (1 Bit)

If the switch object receives a telegram with the value "1", the output will be switched on. In the default settings, the dimming time for switching on is 0,6 s at 100%. The output is switched off with an object value of "0".

The value that is approached when switching on using the switch object, can be defined by means of parameters.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?