MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Reference Position

After a reference movement has been triggered, the drive moves to the desired parameterizable reference position (end position). If you have set both end positions as reference positions, the drive will move to the nearest end position, depending on its current position.

Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

-Blind/roller shutter

Calibration

-Automatic, Locking & Calibration settings

Reference position

Upper

Lower

Upper and lower

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?