MTN6710-0102S / MTN6810-0102 / MTN6805-0008

General Information about the Application

With this software application, you can program the SpaceLogic KNX Dimmer Master. The device can switch and dim ohmic, inductive or capacitive loads. The dimmer is also designed for dimmable LED and energy-saving lamps. You can find information on the connectible loads under Express Settings for Dimming and in the user manual.

The dimmer controls the brightness of the connected lamps. You can set the control functions individually for each output channel of the dimmer.

You can add up to two KNX Universal Dimming Extension or Switch/Blind Extensions to the device. This results in the following combinations:

Master

Extension 1

Extension 2

Outputs

MTN6710-0102S

-

-

2 x dimming

MTN6710-0102S

MTN6810-0102

-

4 x dimming

MTN6710-0102S

MTN6810-0102

MTN6810-0102

6 x dimming

MTN6710-0102S

MTN6810-0102

MTN6805-0008

4 x dimming and
8 x switching or 4 x blind

MTN6710-0102S

MTN6805-0008

MTN6810-0102

4 x dimming and
8 x switching or 4 x blind

MTN6710-0102S

MTN6805-0008

MTN6805-0008

2 x dimming and
16 x switching or 8 x blind

The basic settings of the device are set on the General settings tab. Here you define the device configuration from master and extensions. You can then also specify the functions of the outputs here. (General Settings). The functions of the outputs are parametrized on the Express settings and Extended settings tabs of the outputs for dimming, switching, roller shutter and blind.

Express Settings for Dimming

Express Settings for Switching

Express Settings for Blind/Roller Shutter

Express Settings for Roller Shutter

Extended Settings for Dimming

Extended Settings for Switching

Extended Settings for Blind/Roller Shutter

Extended Settings for Roller Shutter

You can use the Extended settings of the device to configure the global settings of the devices as needed. (Extended Settings).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?