MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Staircase Lighting Time Variable

With Staircase lighting time variable, a time between 0 s and 65 535 s is defined via the object Staircase variable (2 bytes DPT 7.005 time (s)), e.g. using a button. This enables you to specify the length of the staircase lighting time from different places depending on the desired situation.

Ext. 1/2 Output 1-8 -Switch: Switching

Staircase lighting time variable

– Time settings

Manual switching off

Active

Not active

 

Time extension

Not retriggerable

Retriggerable

Retriggerable to the higher value

Retriggerable and adding

   

Max. number of additions

2 (2 - 5)

 

Number of prewarnings

0 (0 - 5)

 

Warning starts (5...255, unit = 1s) before end

20 (5 - 255)

   

Hint: Staircase duration time must be longer or equal than prewarning start time.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?