MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Value Dimming (1 Byte)

The value dimming function is used to set the required brightness directly. To do this, the value object of the output channel sends the desired brightness value as a percentage between 0% and 100%. The value range is divided up into 255 brightness levels. A level has a step value of approximately 0.4%. The telegrams for dimming with absolute values have a 1-byte data format (0 to 255).

The desired brightness values must lie within the limits which are defined by the minimum and maximum dimming values. If the brightness value exceeds the maximum dimming value, the maximum dimming value will be set as the output value. If the brightness value is lower than the minimum dimming value, this will be set as the output value.

The preset dimming time for value dimming from 0% to 100% is 0.6 s.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?