MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Object Values for Alarm

The alarm function is activated if the alarm object receives a telegram with the object value that you defined with the parameter Alarm. The reaction is defined by the parameter Behavior at start of alarm.

If the alarm object receives a telegram with the object value opposite of that for activation, the alarm function is canceled and the output adopts the state that you defined in the parameter Behavior at end of alarm.

At object value “1”:
The object value “1” switches on the alarm function. If the object value “0” is received, the alarm function is switched off again.


At object value “0”:
The object value “0” switches on the alarm function. A telegram with the object value “1” deactivates the function again.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?