MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Works on Object

For each channel, you can parametrize whether the delay affects the switch object, dimming object or value object, or multiple objects in combination.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?