MTN6710-0102S / MTN6810-0102 / MTN6805-0008

PIN Code for Firmware Update

For security reasons, you have to set a valid 4-digit PIN code to block unauthorized updates of the device firmware.

The PIN code defined in the ETS has to be entered in the Schneider-Electric Firmware Update Tool before downloading the firmware. This prevents unauthorized firmware update of the device via the USB interface.

Extended settings

PIN Code for Firmware Update

 

Please enter PIN Code for Firmware Update

(4 digits, 0 ... 9)

1234

PIN codes that are insecure or too simple cannot be selected.

You will receive the following message:

No valid PIN Code for Firmware Update! Please enter a valid PIN Code before you download your configuration!

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?