MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Alarm Function

Alarm Function

Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

-Blind/roller shutter

Alarm function

-Safety and alarm settings

Alarm function

Disabled

Enabled

Alarm

At object value "1"

At object value "0"

Behavior at start of alarm

No reaction

Stop

Up

Down

Move to position

   

Height position at start of alarm in %

0 (0-100)

   

Behavior at end of alarm

No reaction

Up

Down

Move to position prior alarm

Accept current automatic position

   

Behavior after bus voltage recovery

Disabled

Enabled

As before bus voltage failure

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?