MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Dependent Functions and Parameters

Many functions are affected by how other functions are set. This means that dependent functions can only be seen and selected in the ETS when the upstream function is enabled.

  • If you de-select functions or change parameters, previously connected group addresses may be removed in the process.

  • The values of some parameters only become active once the functions influenced by these parameters are activated.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?