MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Express Settings for Switching

On the Express settings for switching tab, define basic settings and activate or deactivate other functions.

To switch electrical loads, you can set the channel function of the device to Switching mode. The operating mode is selected for each output on the Defining Channel Functions tab.

General settings

Channel function Extension 1 / Extension 2 Output 1-2

Switching

   

Ext. 1/2 Output 1-2 -Switch: Switching

Express settings for switching

...

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?