MTN6710-0102S / MTN6810-0102 / MTN6805-0008

Extended Drive Timing

For special drives and blinds, you can adjust the drive times by means of additional parameters.

Ext. 1/2

Output 1+2 / 3+4 / 5+6 / 7+8

-Blind/roller shutter

Extended drive timing

-Extended drive timing

Idle time until upward movement (0...255, unit = 10 ms)

0

   

Startup delay (0...255, unit = 10 ms)

0

   

Deceleration delay (0...255, unit = 10 ms)

0

   

Additional startup time when opening slat downwards (0...255, unit = 10 ms)

0

   

Additional startup time when opening slat upwards (0...255, unit = 10 ms)

0

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?