MTN6710-0102S / MTN6810-0102 / MTN6805-0008

User Interface

In the ETS, the device parameters are opened using the Edit parameters service button.

The user interface is divided into 2 sections: The tabs are on the left and the parameters on the right, together with their values.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?